What We Do Renesas
Renesas High Components, Inc.
HomeCorporateWhat We Do
What We Do Top
* Package Assemblies
* New Products
Mu-chip (RFID)
Business
Trends
Product Line
Tester Line
High-Frequency Modules

HITACHI mu-chip
Explanation of New Products

1. What is the mu-chip (RFID: Radio Frequency IDentification)?

The mu-chip radio automatic identification IC is a 0.4mm microchip. Since data are written on read only memory (ROM) in the manufacturing process, data cannot be rewritten, thus ensuring a high degree of authenticity. In the past, the mu-chip was used in goods management tags at steel distribution sites by taking advantage of the chip's characteristics, such as small size, authenticity and non-contact property. But now, the mu-chip will be embedded into paper for the first time.

Salient Features
Simple functions : read only, no congestion control, individual management capability (low cost)

Data storage : 128 bit unique ID (set at the time of manufacture)
network-based high-grade information management

Characteristics of communication : frequency of 2.45GHz, maximum distance of approximately 30cm (with external antenna)

Passive type : operates without batteries

Conceptual drawing
The mu-chip is actually protected by synthetic resin on the back of the external antenna.

Conceptual drawing Conceptual drawing



2. What is the mu-chip system?
The mu-chip system



3. Business fields of the mu-chip

High security Micro size
High security
The data of the mu-chip consists entirely of unique ID data. Furthermore, since the data cannot be rewritten, security is ensured. Also, as custom codes can be carried, ID management can be geared to the characteristics of each product.
Micro size
Owing to the fact that the mu-chip is 0.4mm2, it can be mounted on paper, parts, and other media and equipment on which the mounting of the mu-chip was previously thought to be difficult. Initiatives will be undertaken to develop new businesses that take advantage of the small size of the mu-chip.
Secure ID management Environment-friendly
Secure ID management
The mu-chip's own security management supports all levels of management of unique ID data, readers and other equipment and application systems. Even if the chip's specifications are upgraded in the future, mixed management can be conducted accordingly.
Environment-friendly
In the 21st century, consideration for the environment is the norm at corporations. The management of recycled parts and materials by means of custom codes will enable the efficient recovery and reuse of resources.



4. A variety of business solutions

[ Paper Solution ]
Reliability and management functions can be enhanced by mounting the chip on paper.
Speedy identificatio Reliable management Prevention of forgery Effective customer management
Speedy identification of various slips Reliable management of tickets, gift certificates and other notes Prevention of forgery by ID management. Reliability is the foremost requirement of certificates. Effective customer management through invitations and direct mail
[ Life cycle Solution ]
Realizes integrated product management for all stages from manufacture to distribution to recycling.
Product delivery and item check Reuse of resources Inventory managemen Stocktaking increases
Speedy and reliable product delivery and item check Reuse of resources through management of parts and materials Efficiency of inventory management and stocktaking increases.
[ Security Solution ]
Reliability is the very basis of business. The mu-chip will be highly effective for checking authenticity.
Greater reliability and security Enhance their reliability ID check Prevention of illegal copying
Lends greater reliability and security to products Can be used to manage financial products and enhance their reliability The basis of security. ID check during entry and exit For the prevention of illegal copying of products on the market


[ Questions concerning the mu-chip ]


To Top To Top
Site MapContact UsCopyright InfoPrivacy Policy